DEMO9S121XXEP100 Setup file for Windows 7 64 bit operating system

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

DEMO9S121XXEP100 Setup file for Windows 7 64 bit operating system

978 次查看
Drake
Contributor II

Demo board drivers will not load in a Windows 7 envorinment. Is there a 64 bit driver version available. My setup files are dated 6/22/2010.The computer suggests getting a 64 bit version software. Is this available? Otherwise is there a work-around for loading the demo software in Windows 7?

标签 (1)
0 项奖励
回复
2 回复数

867 次查看
Drake
Contributor II

I finally got around this by not using the program. I installed the USB Multilink BDM programmer and used the programmer to program and debug my demo board. The system was much more stable. I had to install a connector on the demo board.

0 项奖励
回复

867 次查看
Rodrigo_Cruz
Contributor I

you could use the DEMO board in Windows 7? which connector I have to put on the board?

0 项奖励
回复