Current specification of EVDD pin

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Current specification of EVDD pin

1,399 Views
curious
Contributor I

Hello community,

I am using the EVDD pin of the S12ZVM to provide a 5V supply to an external sensor (Op-Amp). The sensor has a 100n bypass MLCCs in parallel to the supply pins. What is the maximum transient current and the maximum time for the EVDD pin during switch on? The 100n capacitor is being charged during the switch on and the current limit is apparently exceeded for a short period of time. Is it ok to filter the overcurrent protection during this switch on time? In steady state the current consumption is about 3mA.

 

Thank you.

0 Kudos
Reply
1 Reply

1,387 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hello Florian,

As the Absolute maximum ratings specified, the I_EVDD1 instantaneous current must not exceed 80mA.

danielmartynek_1-1600859620916.png

danielmartynek_2-1600859653645.png

Maximum allowed continuous current is 20mA.

danielmartynek_3-1600859742999.png

Regards,

Daniel

 

 

0 Kudos
Reply