Could not find the definition of TIM registers in XET256

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Could not find the definition of TIM registers in XET256

跳至解决方案
1,150 次查看
myles0
Contributor I

Hi:

     I Could not find the definition of each TIM register in "mc9s12xet256.h", such as  "TIM_TIOS, TIM_TCTL4, and so on". Meanwhile , I could not find any definition on the addresses of 0x03D0–0x03FF,which are mapped to the TIM module.They can all be found in "mc9s12xep100.h".My H file version is 3.00.034.

     Should the TIM register definition be finished by user himself when use mc9s12xet256 ?

Original Attachment has been moved to: mc9s12xet256.h.zip

标签 (1)
0 项奖励
回复
1 解答
911 次查看
RadekS
NXP Employee
NXP Employee

Hi 小兵 祝,

It is correct.

Please look at Table D-2. Peripheral Options of MC9S12XE-Family Members in RM.

The TIM module is available only for 9S12XEP100 and 9S12XEP768. The TIM is routed to port R.

Please use ECT timer which is routed to port T.

It is enhanced version of TIM timer (+16-Bit Modulus Down Counter, +Pulse Accumulator B).

I hope it helps you.

Have a great day,
Radek

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

1 回复
912 次查看
RadekS
NXP Employee
NXP Employee

Hi 小兵 祝,

It is correct.

Please look at Table D-2. Peripheral Options of MC9S12XE-Family Members in RM.

The TIM module is available only for 9S12XEP100 and 9S12XEP768. The TIM is routed to port R.

Please use ECT timer which is routed to port T.

It is enhanced version of TIM timer (+16-Bit Modulus Down Counter, +Pulse Accumulator B).

I hope it helps you.

Have a great day,
Radek

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------