Convert Local Address and Global Address on S12XEQ384

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Convert Local Address and Global Address on S12XEQ384

4,383 次查看
huuhuynhchi
Contributor III

Hello All,

I am working with MC9S12XEQ384 but I have some problem with Local Address and Global Address. How can we convert from Local Address to Global Address on MC9S12XEQ384 ?

Thank you so much!

标记 (1)
5 回复数

4,118 次查看
RadekS
NXP Employee
NXP Employee

Hi Huu,

if you need to convert P-Flash address, you may use followed code:

//==============================================================================
//Convert_Ppage2Global
//==============================================================================
unsigned long int Convert_Ppage2Global(unsigned long int Addr)
{    
  Addr = ((Addr>>2) & 0x003FC000UL) | (Addr & 0x00003FFFUL) | 0x00400000;
  return(Addr);
}

Attached is S12XE memory map in excel sheet for your reference.

I hope it helps you.

Have a great day,
Radek

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

4,118 次查看
huuhuynhchi
Contributor III

Thank Radek,

Your information is very useful for me :smileyhappy: And for the RAM area, do we have the function to convert to Global address like P-Flash ?

4,118 次查看
RadekS
NXP Employee
NXP Employee

Hi Huu,

that is even easier:

//==============================================================================
//Convert_Rpage2Global
//==============================================================================
unsigned long int Convert_Rpage2Global(unsigned long int Addr)
{    
  Addr = ((Addr & 0x00FF0000UL)>>4) | (Addr & 0x00000FFFUL);
  return(Addr);
}

I hope it helps you.

Have a great day,
Radek

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

4,118 次查看
huuhuynhchi
Contributor III

Thank Radek,

I have a concern, How can we use the RPAGE area ? How to initiate it to store data or code ?

0 项奖励
回复

4,118 次查看
RadekS
NXP Employee
NXP Employee

Hi Huu,

As first, I would like to recommend look at our application note AN3784 Understanding the Memory Scheme in the S12(X) Architecture

http://www.nxp.com/files/soft_dev_tools/doc/app_note/AN3784.pdf

After that, please look at TN238 and TN240 PDFs in "c:\Program Files (x86)\Freescale\CWS12v5.2\Help\pdf\" directory.

 

In short, you may use linker directive “#pragma DATA_SEG” for placing variables into paged RAM. For example:

#pragma DATA_SEG PAGED_RAM

unsigned int my_counter = 0x1234;

//…

#pragma DATA_SEG DEFAULT

Note: PAGED_RAM section is defined by default in prm linker file. You may create your own section.

Note: You must add the option -D__FAR_DATA on the compiler command line for proper paged RAM variables initialization during startup.

Note: The #pragma CONST_SEG change default linker settings for constants. The #pragma CODE_SEG change default linker settings for code placement.

I hope it helps you.

Have a great day,
Radek

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复