Compatibility of an RTOS and mc9s12p12

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Compatibility of an RTOS and mc9s12p12

843件の閲覧回数
karimaaissaoui
Contributor II

I wonder if the mc9s12p12 freescale microcontroller can support a real-time operating system? If so what kind of RTOS that can be supported?

Regards.

ラベル(1)
0 件の賞賛
返信
1 返信

741件の閲覧回数
RadekS
NXP Employee
NXP Employee

Hi Karima,

Unfortunately mc9s12p12 doesn’t have any direct RTOS support from NXP side. However there exist several third party RTOS platforms which could be used on this MCU.

Currently most popular RTOS is probably FreeRTOS:

http://www.freertos.org/index.html

This article shows adding implementation FreeRTOS as Processor Expert component:

http://mcuoneclipse.com/2012/02/11/back-to-classic-freertos-for-freescale-s12x/

Other possible RTOS for S12 devices:

ERICA Enterprise

http://erika.tuxfamily.org/drupal/

http://erika.tuxfamily.org/wiki/index.php?title=Freescale_S12

Micrium uC/OS

http://micrium.com/

Trampoline Operating System

http://trampoline.rts-software.org/?lang=en

Be aware that mc9s12p12 has just 6kB of RAM, so RTOS implementation will be probably mainly limited from this side.


I hope it helps you.

Have a great day,
RadekS

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信