Code Warrior for 9S12XDP512?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Code Warrior for 9S12XDP512?

跳至解决方案
1,683 次查看
roberthiebert
Senior Contributor I

Which version of Code Warrior Special Edition should I be using for use with the 9S12XDP512? Looking at the selections offered I couldn't find one that specified this particular target.

标签 (1)
0 项奖励
回复
1 解答
1,530 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

you are welcome! if you regard this thread is solved, please help us to mark the correct and helpful answer, thanks!

在原帖中查看解决方案

0 项奖励
回复
7 回复数
1,530 次查看
BlackNight
NXP Employee
NXP Employee
0 项奖励
回复
1,530 次查看
roberthiebert
Senior Contributor I

Thanks Erich, but when I go here

Special Edition Software

and look at the info on CW12V5.1, the 9S12XDP512 is not on the list of supported microcontrollers, or am I missing it somewhere?

0 项奖励
回复
1,530 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

i think you should click "i" icon of the item in

http://www.freescale.com/webapp/sps/site/overview.jsp?code=CW_SPECIALEDITIONS

this is the "new feature" of CW5.1, but not all the 5.1 features.

CW5.1 can well support all HC12,HCS12 and HCS12X family chips.

----------------------------------------------------------------------------------------------------------------------------------------------------------

CodeWarrior Development Studio for S12(X) Microcontrollers V5.1 adds the following new features: 

  • Optimization features to improve page management
  • Support for the following microcontrollers:  Support for Open Source BDM connection on S12(X) Tower boards
    • MC9S12G128, MC9S12G96
    • MC9S12GN16, MC9S12GN32
    • MC9S12I128
    • MC9S12XB256
    • MC9S12XHY128, MC9S12XHY256
    • MC9S12XHZ256, MC9S12XHZ384
  • Support for Windows 7 (32-bit and 64-bit platforms)
  • Support for Windows XP and Windows Vista (64-bit platforms)
0 项奖励
回复
1,530 次查看
roberthiebert
Senior Contributor I

I did click the "i" icon but didn't , and still don't see any mention of the 9S12XDP512.

No matter. If you say it will work then that's the answer I was looking for.

Thanks

0 项奖励
回复
1,530 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

you are correct there is no mention if click i button. it only mentioned the new feature and improvement. all features are listed in its main page: http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CW-HCS12X&tid=CWH

0 项奖励
回复
1,530 次查看
roberthiebert
Senior Contributor I

Thanks.

0 项奖励
回复
1,531 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

you are welcome! if you regard this thread is solved, please help us to mark the correct and helpful answer, thanks!

0 项奖励
回复