I want to use simple cheme with max232, maybe attiny2313 and connect by COM port to this cheme, and use it for programming
HCS12. Can do it, while i not have near me programmer from shop? For example connect to BDM and reset pins.
And which soft i can use for this?
解決済! 解決策の投稿を見る。
Best way is BDM. Best and chip BDM solution - open source BDM pjt USBDM. There is all circuits, soft, etc.
Hi,
you can program though the serial port but you first would have to download a serial bootloader program into your board / target, using for instant another BDM Programmer. Once that this bootloader program resides in your board/target, you could reprogram the rest of the memory via the serial port. But one first programming using a BDM is needed. Please note that a serial bootloader allows only to program the memory, but you won't be able to debug your code via the serial port.
Hi,
Thanks for your answer!
But please explain litle bit more:
1. i can develop simple scheme to connect for mc9s12 (hcs12), like using rs232, max232 or
avr attiny, and connect it to serial port, right?
2. which programm you recommend me for this purpose? Maybe Code warrior support this, or i need
write code by myself for programming on my own circuit? In another words have it already solution?
Right now i not near city, but i need repair few things, and need to connect with HCS12, so i thing
how i can do it here without any famous programmers like ETL, xprog etc.
Best way is BDM. Best and chip BDM solution - open source BDM pjt USBDM. There is all circuits, soft, etc.