CAN connector on EVB9S12XEP100 and DEMO9S12XEP100

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CAN connector on EVB9S12XEP100 and DEMO9S12XEP100

2,088件の閲覧回数
ChrisN
Contributor II
The boards for the S12XE have CAN connectors which are different from the DB9 that is "normally" used. Could someone shed light on which type this connector is and where I can obtain some?

Thanks,
Chris
ラベル(1)
0 件の賞賛
返信
2 返答(返信)

479件の閲覧回数
allawtterb
Contributor IV
The CAN connectors and LIN connectors on both boards look like they are Molex connectors.  They look like the same connectors as the CAN and LIN connectors on the SK-S12XDP512-A which has a BOM on the softec site.  The CAN connectors look to be part # 39-30-3047, you can find them on Molex's website which should be able to give you a mating connector and what distributors have them in stock.
 
- Brett
0 件の賞賛
返信

479件の閲覧回数
ChrisN
Contributor II
Thanks, Brett. The mating connector appears to be Molex 39-01-4040 and one needs the housing plus four female contacts with the plating of your choice. The following Mouser catalog page has a good overview:

http://www.mouser.com/catalog/634/1424.pdf

Chris

0 件の賞賛
返信