CAN can't be used on development board DEVKIT-S12XE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CAN can't be used on development board DEVKIT-S12XE

3,358 Views
zoejiang
Contributor I

Hello,

I have bought two DEVKIT-S12XE development boards. Quick start package also download from web side.

Connect two boards as document 'DEVKIT-S12XE Lab Examples and Board Overview', page 6. Download the software in folder 'Lav4_CAN_S12XE ' into one board, and simulate in the other board.

Can bus can't be connected successfully between two boards.

Can signal can't be read by oscilloscope.IMG_0177.JPG

Labels (1)
0 Kudos
Reply
11 Replies

2,947 Views
aaronlee
Contributor V

Do you mount 0 ohm resistor to R94?

0 Kudos
Reply

2,947 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi,

How do you supply the boards? I think there is a short R94 – C17.

Are you sure both MCUs are running? Have you tried debugging it?

 

Regards,

Daniel

0 Kudos
Reply

2,947 Views
zoejiang
Contributor I

Yes, I did.

R94 has already been connected by a jumper.

Both boards are running.

Every time I tried I downloaded software both.

Voltage between CAN_H and GND is 0.33V, CAN_L and GND is also the same.

I also measured the voltage between Pin105 and GND , Pin104 and GND, both of them are 4.7v.

I also debugged it, the chip running smoothly.

Main function has been changed to send signal non stopped, but the signal still can't be caught by oscilloscope.

0 Kudos
Reply

2,947 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi,

 

I have downloaded the example code without any modification into DEVKIT S12XE (we have only one board) and measured:

TXCAN0 (PT17)

CAN_tx.png

and the on CAN_H/L (both open)

CAN_PHY.png

  /* Creation of CAN frame */
  id = 0x50;                         /*  Message id               */
  data_send = 0x01;           /*  Data to be send        */
  SendFrame_CAN(id,&data_send, 1);

In idle state, you should have a recessive level 2,5V on both CAN_H/L.

Are you sure there is no short on the boards after your soldering?

Regards,

Daniel

0 Kudos
Reply

2,947 Views
zoejiang
Contributor I

Hello,

Thank you for your reply.

Hard ware engineer and I tried it again. And we found TP13( port 5V-3)  is always 0V during software running. We checked the signal of SPI set in soft ware.  But we still have no idea.

Can you give me an e-mail about the software you tried?

Or give me some information about how to make TP13 5V?

0 Kudos
Reply

2,947 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hello,

I use the example code from DEVKIT-S12XE page.

DEVKIT-S12XE Quick Start Package/…/LAB4_CAN_S12XE

Is the System Basis Chip MCZ33903 supplied (PT2 = 12V)?

Have you tried running only one board as I did?

Does it mean that you have the same problem on both boards?

 

Regards,

Daniel

2,947 Views
zoejiang
Contributor I

Thank you for your help.

Hardware engineer and I finally find we used the wrong power.

Now the problem is solved.

0 Kudos
Reply

2,947 Views
christianhdz
Contributor II

Hi, what is the correct way to power it? I tried using the SWUSB-VDD jumper, since I download the SW using the USB port, but also I need to power the LIN terminal... just VBAT(12V on the LIN pin2,  otherwise it would not communicate on CAN.

0 Kudos
Reply

2,947 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi,

You can power the S12XE MCU via the USB (5V). But you need 12V (VBAT, J9, J8, J12) for MCZ33903CD (SBC) which contains CAN, LIN transceivers and power regulators. In this case, you can supply the S12XE (VDD) from P5V0_SBC (J13).

Regards,

Daniel

0 Kudos
Reply

2,947 Views
tuandongvt
Contributor I

Dear Daniel, Zoe Jiang,

I meet the same problem, i solder short R94,  connect jumper j13.2 and j13.3
CANH/LOW is 0V, 
TP2 is 5V
TP13 is 0V
only user power supply J9 is 5V.
follow you I need to push12V in J9?
Please help me,

0 Kudos
Reply

2,947 Views
tuandongvt
Contributor I

I known problem. I need to connect 12V connect with J9. Then problem is solved.

0 Kudos
Reply