CAN Conformance Testing in MC9S12B128

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CAN Conformance Testing in MC9S12B128

2,434件の閲覧回数
sathees
Contributor I
Dear All,
 
I would like to know if the CAN Controller in the MC9S12B128 micro has been tested according to Conformance Tests as per ISO16845? Please find below some of the requirements of the test:
 
  • Valid frame format class
  • Error detection class
  • Active error frame management class
  • Overload frame class
  • Passive error state and bus-off class
  • Bit-timing class

     

    Thanks and Regards,

    Sathees



    Message Edited by sathees on 2007-10-19 08:53 AM
    ラベル(1)
    0 件の賞賛
    返信
    1 返信

    1,038件の閲覧回数
    Alban
    Senior Contributor II
    Hello,

    The S12B128 had its msCAN module tested on another reference.
    One conformance testing applies to all devices with the same CAN module revision.

    There is one exception to conformance described in the errata sheet: MUCts03570

    The test also covered additional parts which are outside the ISO scope but important.

    Cheers,
    Alban.
    0 件の賞賛
    返信