C++ support for S12ZVL in CodeWarrior for MCU v11.1

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

C++ support for S12ZVL in CodeWarrior for MCU v11.1

ソリューションへジャンプ
1,549件の閲覧回数
michiel-inspiro
Contributor I

Hello,

Is there support for C++ for the S12ZVL microcontroller in CodeWarrior for MCU v11.1? When I generate an example project through New > Bareboard Project and select C++ I get a project that does not compile. See the image below for the error.

Screenshot 2022-06-17 161000.png

Kind regards,
Michiel

0 件の賞賛
返信
1 解決策
1,519件の閲覧回数
stanish
NXP Employee
NXP Employee

Hi Michiel,

C++ compiler is licensed and it is available in Professional Edition license only.

If you open the license.dat file located in "<CW home directory>\MCU\license.dat" you should see :

 

INCREMENT ProfessionalEditionMCU metrowks 11.1...

 

 

for more details please see the CodeWarrior Quick Reference Guide: https://www.nxp.com/docs/en/fact-sheet/950-00437.pdf

 

Hope it helps.

Stan

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,520件の閲覧回数
stanish
NXP Employee
NXP Employee

Hi Michiel,

C++ compiler is licensed and it is available in Professional Edition license only.

If you open the license.dat file located in "<CW home directory>\MCU\license.dat" you should see :

 

INCREMENT ProfessionalEditionMCU metrowks 11.1...

 

 

for more details please see the CodeWarrior Quick Reference Guide: https://www.nxp.com/docs/en/fact-sheet/950-00437.pdf

 

Hope it helps.

Stan

0 件の賞賛
返信