Are there 6 independent PWM programs for S9ZVML128?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Are there 6 independent PWM programs for S9ZVML128?

1,355 Views
panda2022
Contributor II

I want to implement 6 independent output PWM on S9ZVML128.

0 Kudos
Reply
4 Replies

1,220 Views
panda2022
Contributor II

或者我该怎么配置寄存器,我现在一头雾水

0 Kudos
Reply

1,222 Views
panda2022
Contributor II

我想要6路独立的pwm输出到GDU上,有相应的程序吗?

0 Kudos
Reply

1,337 Views
lama
NXP TechSupport
NXP TechSupport

Hi,

ZVML128 provides you to use 6 independent PMF channels (enhanced motor control oriented PWM with fault protection) if you do not use GDU module and connects PMF to GPIO pins. If you use GDU module then it blocks simultaneous active top and bottom part of the H bridge leg (complementary pair). Also, you can use TIM module to generate 4 independent simple PMW.

 

Note, S12ZVL64 or S12ZVL128 provide 8x16 bit PWM channels but simple PWM.

Best regards,

Ladislav

 

0 Kudos
Reply

1,339 Views
zhangp973
Contributor II

不是自带六路PWM输出么  build in 6 channel PWM module 

 

Doesn't it come with six PWM outputs? build in 6 channel PWM module
0 Kudos
Reply