Analog to digital in EVB9S12NE64

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Analog to digital in EVB9S12NE64

4,088 Views
ibrahim2110
Contributor I
hi i've a problem with atd in EVB9S12NE64 i want to make the V refernce high to be 5volt (extrnaly)  instead of the 3.3 v supplied internaly by the kit
idon't know if the atd channels can withstand that 5volt
please if any one know how to do that reply me.
thanks for ur help
Labels (1)
0 Kudos
Reply
2 Replies

1,142 Views
EMontanez
NXP Employee
NXP Employee
For the NE64:

ATD references -

VRL: min = VSSA, max = VDDA/2
VRH: min = VDDA/2, max = VDDA

Where, VDDA: min = 3.135, max = 3.465. Therefore, a 5V ATD reference is not allowed. This kind of reference will cause internal diodes on these ATD pins to clamp.
0 Kudos
Reply

1,142 Views
peg
Senior Contributor IV
Hi,
The supply to the analogue section is generally the same voltage level as the main chips supply. (just cleaner hopefully)
If you want to measure voltages greater than this generally you use a resistive voltage divider into a rail-to-rail non-inverting op-amp connected to the ATD input.
The divider changes the 5V to 3 or so volts, then the buffer which is fed from the same analogue supply as the micros ADC section buffers it and provides a low source impedance to the ADC.
 
Hope that helps
Peg
0 Kudos
Reply