Action of S12ZVM High-Side Driver

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Action of S12ZVM High-Side Driver

跳至解决方案
536 次查看
ikkishingu
Contributor II

Dear person in charge,

 

Hello,

Could I ask a question for just clarification?

 

This is the schematic circuit of GDU HSFET driver on S12ZVM.

Question 1:

After this driver turns off, "Driver off" Transistors(T3&T4) turn on to discharge the external FET.

Is my understand("Driver off" Tr action & the purpose of the Tr) correct?

 

Question 2:

Gate driving speed of "Driver off" is adjustable like a slew rate control?

19671_19671.pngS12ZVM_HSFET_Driver.png

 

Best Regards,

Ikki

标签 (1)
标记 (1)
0 项奖励
1 解答
385 次查看
DPB
NXP Employee
NXP Employee

Hello Ikki

To question (1). Yes, T3 and T4 turn on to switch off the external FET.

To question (2). No, the driver off is not adjustable like a slew rate control.

The driver on slew rate can be adjusted, the driver off is fixed and specified as tHGOFF in the electrical parameter section.

Regards

DPB

在原帖中查看解决方案

0 项奖励
2 回复数
386 次查看
DPB
NXP Employee
NXP Employee

Hello Ikki

To question (1). Yes, T3 and T4 turn on to switch off the external FET.

To question (2). No, the driver off is not adjustable like a slew rate control.

The driver on slew rate can be adjusted, the driver off is fixed and specified as tHGOFF in the electrical parameter section.

Regards

DPB

0 项奖励
385 次查看
ikkishingu
Contributor II

Dear DPB-san,

Thank you for your info.

It makes sense to me!

Ikki

0 项奖励