Action of S12ZVM High-Side Driver

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Action of S12ZVM High-Side Driver

ソリューションへジャンプ
545件の閲覧回数
ikkishingu
Contributor II

Dear person in charge,

 

Hello,

Could I ask a question for just clarification?

 

This is the schematic circuit of GDU HSFET driver on S12ZVM.

Question 1:

After this driver turns off, "Driver off" Transistors(T3&T4) turn on to discharge the external FET.

Is my understand("Driver off" Tr action & the purpose of the Tr) correct?

 

Question 2:

Gate driving speed of "Driver off" is adjustable like a slew rate control?

19671_19671.pngS12ZVM_HSFET_Driver.png

 

Best Regards,

Ikki

ラベル(1)
タグ(1)
0 件の賞賛
1 解決策
394件の閲覧回数
DPB
NXP Employee
NXP Employee

Hello Ikki

To question (1). Yes, T3 and T4 turn on to switch off the external FET.

To question (2). No, the driver off is not adjustable like a slew rate control.

The driver on slew rate can be adjusted, the driver off is fixed and specified as tHGOFF in the electrical parameter section.

Regards

DPB

元の投稿で解決策を見る

0 件の賞賛
2 返答(返信)
395件の閲覧回数
DPB
NXP Employee
NXP Employee

Hello Ikki

To question (1). Yes, T3 and T4 turn on to switch off the external FET.

To question (2). No, the driver off is not adjustable like a slew rate control.

The driver on slew rate can be adjusted, the driver off is fixed and specified as tHGOFF in the electrical parameter section.

Regards

DPB

0 件の賞賛
394件の閲覧回数
ikkishingu
Contributor II

Dear DPB-san,

Thank you for your info.

It makes sense to me!

Ikki

0 件の賞賛