Accessing DS 26521 or 265xx via SPI Bus

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Accessing DS 26521 or 265xx via SPI Bus

1,201 次查看
ASMeti
Contributor I

Hi All,

I have few questions.

I am using DS26521 as slave device and SPI bus in Master mode on MPC 8323 Processor.

1. Wanted to Access DS Chip via SPI ... How can i do that ?

2. Basically wanted to access DS chip via SPI ?

3. Is there any commands/Functions to set or reset the register DS chip registers VIA SPI BUS? (Or in General any device via SPI)

标签 (1)
0 项奖励
回复
1 回复

805 次查看
something
Contributor I

I have done the programming to access the DS26521 using SPI in LPC1114

if you want it tell me on hgc.8421@gmail.com

0 项奖励
回复