About the GDU compoment of MC9S12ZVML128MKH

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About the GDU compoment of MC9S12ZVML128MKH

665 Views
Fan_xy
Contributor III

Hello ,

the chip is MC9S12ZVML128MKH,   CW10. 6.4

In the configuration of the Init_GDU, the “Current sense amplifier” can not be disabled or the “Amplifier

Output” can not be disabled , does this is a bug or it is sure can not disabled ?

I want to use the pin “PAD5_KWAD5_AN1_0_AMP1” as AD channel , while  in the

“Init_GDU” can not disable this pin .

145674_145674.pngpastedImage_0.png

 

 

 

Thank you very much !

Fan

Labels (1)
0 Kudos
1 Reply

443 Views
iggi
NXP Employee
NXP Employee

Hi,

the ADC function has priority over the AMP function on this pin. See Table 1-9. Pin Summary in the latest datasheet.

Therefore the the external pin can be used as ATD input channel, The Current Sense Amplifier (CSA) feature in GDU should be disabled in such case.

Btw, the CSA output voltage can be routed to ADC channel internally. Check  the chapter 18.4.8 Current Sense Amplifier and Overcurrent Comparator in the MC9S12ZVM ref.manual.

So the usage depends on your application and measurements you plan to do.

Regards,

iggi

0 Kudos