AN4258 with S12G128

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

AN4258 with S12G128

2,814件の閲覧回数
ziomocci
Contributor IV

Hi everybody,

 

We are testing AN4258 on an TWR-S12G128, and we are finding troubles with RS232 reception. We have noticed that only disconnecting hyperterminal, bytes are correctly received on EVB side.

Data reception on hyperterminal side is correct, but also connecting directly TX/RX header pins or using two EVB connected between them, everything work correctly (a compare between tx/rx buffer show that).

Did anyone find same problem?

Attached files show our hyperterminal configuration, as suggested on ch 5.3 of AN4258, rev 0, 02/2011

Thank you in advance,

 

BR

 

Andrea Mocci

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

2,510件の閲覧回数
iggi
NXP Employee
NXP Employee

Hi,

The most probably there is a problem with the MCU pin which is connected to /FORCEOFF pin of MAX3387E transciever. The MCU pin is floating, so the transciever gets on and off randomly.

The solution can be to hardwire the /FORCEOFF pin to VDD.

Other solution can be to modify the StartS12.s file located in Sources folder of the Bootloader_S12 application SW.

The MCU pin PAD15 should be set as digital output by write to DDR0AD register and then set high level at the pin by write to PTA0AD register:

This is how it should look like:

   ; TWR-S12G128 - pin PAD07 - pushbutton SW4
 
  movb  #$80, $0274     ; pin PAD15 as digital output (DDR0AD register) for drive FORCEOFF* signal at RS232 transceiver
  movb  #$80, $0270     ; set hi level at pin PAD15 (PT0AD register) for enable RS232 transceiver
 
  movb  #$80, $0279     ; enable pull up resistor on pin PAD07 (button SW4)

  movb  #$80, $007D     ; enable digital input buffer on pin PAD07 (button SW4)
           
   nop   ;wait a few cycles for stabilization of the signal
   nop
   nop
   nop
   nop
 
  brclr $0273, $80, GoBoot  ; if PAD07 == 0 then start the bootloader
                            ; if PAD07 == 1 then start the application
                           
  movb  #$00, $007D   ; disable digital input buffer on pin PAD07
  movb  #$00, $0279   ; disable pull up resistor on pin PAD07 - restore default state
                      ; keep the PAD15 high
  ; ---------------------------------------------------------------------------------

Hope that helps.

Regards,

iggi

0 件の賞賛
返信