A question about the use of the function GFLIB_ControllerPIrAW

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

A question about the use of the function GFLIB_ControllerPIrAW

ソリューションへジャンプ
1,997件の閲覧回数
maxxu
Contributor IV

Hi

   I'm designing a BLDC driver ,with Automotive Math and Motor Control

   Library Set for NXP MC9S12ZVM

  I have three questions about Function GFLIB_ControllerPIrAW

1、Are there three functions here, and what is the relationship between them

    (1)Function GFLIB_ControllerPIrAW;

    (2)Function GFLIB_ControllerPIrAW_F32;

    (3)Function GFLIB_ControllerPIrAW_F16;

2、How to distinguish "differentiation methods"?

    (1) “Trapezoidal”,

    (2)“Backward Rect”,

    (3)“Forward Rect”

      Which one is used in “S12ZVML-MINIBRD_BLDC_Sensorless_CW_IDE” ?

      I think it's using the “Forward Rect”,then,But put the parameters in the formula

 
 

maxxu_2-1612363961743.png

    The result is

               u(k) = u(k-1) + KP*(e(k)-e(k-1)) + KI*Ts*e(k-1),

    However,The standard formula of discrete PI is

               u(k) = u(k-1) + KP*(e(k)-e(k-1)) + KI*Ts*e(k),

    The two formulas are not the same. Is there something wrong with my deduction

3、  What is the specific meaning of f32acc and f16inerrk1?

        f32acc

        f16inerrk1

        There is no detailed description of the document, which I can't understand

 

Hope to get the help of experts, thank you very much!

0 件の賞賛
返信
1 解決策
1,981件の閲覧回数
petrz_
NXP Employee
NXP Employee

Hi maxxu,

the difference between GFLIB_ControllerPIrAW, GFLIB_ControllerPIrAW_F16, and GFLIB_ControllerPIrAW_F32 is described in the AMMCLib User's Guide, chapter 1.3 "Multiple Implementation Support". We recommend to use the F16 implementation on S12ZVM since it is the fastest.

Parameters of the AMMCLib function GFLIB_ControllerPIrAW can be calculated using any of the discretization methods: trapezoidal, backward rectangular, and forward rectangular. Table 119 in the chapter 2.22 "Function GFLIB_ControllerPIrAW" in the AMMCLib User's Guide specifies how to calculate coefficients CC1 and CC2 with each of the three discretization methods.

For example, the coefficients for the backward rectangular method are listed as

petrz__0-1612515545595.png
petrz__1-1612515545598.png

If you substitute CC1 and CC2 in the equation GFLIB_ControllerPIrAW_Eq3, you get

petrz__2-1612515545608.png

which corresponds to what you call "standard formula of discrete PI".

If you know the desired gains Kp and Ki and the sampling period Ts, you can use any of the discretization methods to calculate the constants CC1 and CC2. The microcontroller will run the same program regardless of which discretization method you use - it is a design consideration, not a program feature. The example code for S12ZVML-MINIBRD_BLDC_Sensorless_CW_IDE comes with a set of numerical values for constants CC1 and CC2 without specifying what particular method was used to design them.

Tuning of the controller parameters can be done conveniently during the run of the motor using the FreeMASTER tool with the preset S12ZVMLMINIBRD_BLDC_SW_CW11.pmp which is provided in the S12ZVM Mini Board SW package.

Function GFLIB_ControllerPIrAW_F16 keeps its state variables in a structure pointed to by the API pointer pParam. The description of the function API in chapter 2.22.2 "Function GFLIB_ControllerPIrAW_F16" in the AMMCLib User's Guide specifies the type of this pointer GFLIB_CONTROLLER_PIAW_R_T_F16. You can simply click on this type in the Table 121, which will bring you the chapter 5.55 which provides detailed description of the structure members:

Type

Name

Description

tFrac32

f32Acc

State variable - internal controller
accumulator.

tFrac16

f16InErrK1

State variable - controller input from the
previous calculation step.

These state variables are automatically initialized when you call function GFLIB_ControllerPIrAWInit, see chapter 2.22.3 for details.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,982件の閲覧回数
petrz_
NXP Employee
NXP Employee

Hi maxxu,

the difference between GFLIB_ControllerPIrAW, GFLIB_ControllerPIrAW_F16, and GFLIB_ControllerPIrAW_F32 is described in the AMMCLib User's Guide, chapter 1.3 "Multiple Implementation Support". We recommend to use the F16 implementation on S12ZVM since it is the fastest.

Parameters of the AMMCLib function GFLIB_ControllerPIrAW can be calculated using any of the discretization methods: trapezoidal, backward rectangular, and forward rectangular. Table 119 in the chapter 2.22 "Function GFLIB_ControllerPIrAW" in the AMMCLib User's Guide specifies how to calculate coefficients CC1 and CC2 with each of the three discretization methods.

For example, the coefficients for the backward rectangular method are listed as

petrz__0-1612515545595.png
petrz__1-1612515545598.png

If you substitute CC1 and CC2 in the equation GFLIB_ControllerPIrAW_Eq3, you get

petrz__2-1612515545608.png

which corresponds to what you call "standard formula of discrete PI".

If you know the desired gains Kp and Ki and the sampling period Ts, you can use any of the discretization methods to calculate the constants CC1 and CC2. The microcontroller will run the same program regardless of which discretization method you use - it is a design consideration, not a program feature. The example code for S12ZVML-MINIBRD_BLDC_Sensorless_CW_IDE comes with a set of numerical values for constants CC1 and CC2 without specifying what particular method was used to design them.

Tuning of the controller parameters can be done conveniently during the run of the motor using the FreeMASTER tool with the preset S12ZVMLMINIBRD_BLDC_SW_CW11.pmp which is provided in the S12ZVM Mini Board SW package.

Function GFLIB_ControllerPIrAW_F16 keeps its state variables in a structure pointed to by the API pointer pParam. The description of the function API in chapter 2.22.2 "Function GFLIB_ControllerPIrAW_F16" in the AMMCLib User's Guide specifies the type of this pointer GFLIB_CONTROLLER_PIAW_R_T_F16. You can simply click on this type in the Table 121, which will bring you the chapter 5.55 which provides detailed description of the structure members:

Type

Name

Description

tFrac32

f32Acc

State variable - internal controller
accumulator.

tFrac16

f16InErrK1

State variable - controller input from the
previous calculation step.

These state variables are automatically initialized when you call function GFLIB_ControllerPIrAWInit, see chapter 2.22.3 for details.

0 件の賞賛
返信