I am working on MC9S12ZVL and have a question about the restart mode of ADC12B_LBA.
It is said that after the execution of EOL command a restart event is required to start the conversion from top of CSL. However, I find that the CMD_SEL can be 0b10 which means a EOL command to automatically wrap to top of CSL and continue conversion. The two statements seems to be in conflict. Can someone help me to figure out which one is right?
Hi,
The restart event start a conversion sequence from the top of the CSL, however, there are two types of possible conversions. The first one is a single CSL processing, where new restart event must be initiated to start a new sequence. The other one is restart event which starts continuous mode of conversions from the top of the list.
The first mode is used if you want to perform one ATD sequence and then process a data set. The other one is used if I do not care about moment of conversion and I need only data from last conversion set. In this case I do not have to start conversion set again and it is performed continuously but I do not have possibility of controlling exact timing of conversions so I am able only to read last data.
Best regards,
Ladislav
Hi Ladislav,
Thanks for your reply. It is very helpful. I find the continuous mode is introduced to be used in trigger mode in the manual. So the continuous mode is also available in restart mode? It feels like the main difference between restart mode and trigger mode is a restart event is followed by a trigger event in restart mode. I am thinking if this simplified control in restart mode really saves more resources or improves efficiency. Can you solve my questions about restart mode?
Best regards,
CK
Hi,
Have you read chapter 10.9.7.x Conversion flow control application information.
Best regards,
Ladislav