9S12XEG384 bank F9 is not programmed

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

9S12XEG384 bank F9 is not programmed

跳至解决方案
736 次查看
leroy_o
Contributor III

I have a problem with the flashing of the F9 flash memory bank after having switched a project from 9S12XEG128 to 9S12EG384 recently.

 

The F9 flash memory bank is declared in the prm project file, also, F9 memory locations appear in the project.abs.s19 file, but this code is not programmed in actual flash memory.

 

I use a Freescale PE USB multilink interface to perform the actual flashing, it worked with the 9S12XEG128, but after flashing, object code in the F9 bank appear as "FFFFFFFFFFFFFFFF...".

 

Has someone encoutered the same kind of problem and solved it?

标签 (1)
标记 (3)
0 项奖励
回复
1 解答
586 次查看
leroy_o
Contributor III

I solved the problem:

I forgot to also perform in HCS12MultilinkCyclone Pro:

- Select derivative

    - MC9S12XEQ384


Problem solved.

在原帖中查看解决方案

0 项奖励
回复
1 回复
587 次查看
leroy_o
Contributor III

I solved the problem:

I forgot to also perform in HCS12MultilinkCyclone Pro:

- Select derivative

    - MC9S12XEQ384


Problem solved.

0 项奖励
回复