9S12XEG128 controller: MPU, XGATE work together problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

9S12XEG128 controller: MPU, XGATE work together problem

671 Views
prasadgarge
Contributor I

I am using 9S12XEG128 controller. I successfully established communication with sensor through XGATE, SPI.

However, now when I try to configure MPU (first application triggered MPU self test and then proper operation), then XGATE software error interrupt gets generated.

So, I refer "Software error interrupt" related pdf, I can find I have to configure RAMWPC, RAMXGU, RAMSHU, RAMSHL registers for defining XGATE, CPU, shared RAM areas.

However, when I try to find above mentioned registers I could not find them in controller's register definition file. Also, in other pdfs found over net, these mentioned registers addresses coincide with MPUDESC2, MPUDESC3, MPUDESC4, MPUDESC5 registers. Please suggest how to access RAMWPC, RAMXGU, RAMSHU, RAMSHL registers or what could be other problem.

Labels (1)
0 Kudos
Reply
1 Reply

483 Views
lama
NXP TechSupport
NXP TechSupport

Please look at the chapter 4.3 in the

http://cache.freescale.com/files/microcontrollers/doc/app_note/AN3242.pdf

"4.3 RAM Protection

The RAM protection configuration registers in the S12XD MMC (RAMWPC, RAMXGU, RAMSHL and

RAMSHU) do not exist on the S12XE. The functionality of these S12XD registers is now part of the MPU

  1. See Section 11.2, “MPU Access Violation Vector”."

Best Regards, Ladislav

0 Kudos
Reply