9S12XDP512 SCI1 Libraries - Sample IO

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

9S12XDP512 SCI1 Libraries - Sample IO

1,881件の閲覧回数
Brian
Contributor I
I've spent the better part of two days trying to get various samples of code for the 9S12DP256 working on the 9S12X with no luck, for the secondary serial IO port (SCI1). (this is for the Technological Arts 9S12X board).

What I would like to be able to do is find some "plug n play" code that I can use as a basis for developing my own programs for serial IO. I would like to be able to communicate with the board via serial (both input and output).

I have tried some SCI programs and tried just about everything I could find on the web, but I simply get either just a dead terminal (using hyperterminal for example) or after heavy modification, a bunch of junk.

Does anybody have a Codewarrior project for the 9S12X that I can simply load onto the board and should allow at the least, serial output, but preferably also input? Thanks.
ラベル(1)
0 件の賞賛
返信
2 返答(返信)

712件の閲覧回数
Ilocano
Contributor I
I have written some sample codes to be found here.
See if they are of any use. In the sample code are SCI routines.
0 件の賞賛
返信

712件の閲覧回数
Ilocano
Contributor I
Sorry about that (new to this forum) the link is
http://support.technologicalarts.ca/docs/Adapt9S12X/
0 件の賞賛
返信