9S12X ATD0 and ATD1 clock rates are different

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

9S12X ATD0 and ATD1 clock rates are different

3,347 Views
dwhite
Contributor I
CPU: S912XDT256 mask 1M84E running at 40MHz
Compiler: CodeWarrior v4.5
 
 
PROBLEM:
I'm configuring ATD0 and ATD1 exactly the same way but ATD1 runs at half the speed of ATD0.
 
Both ATD modules are configured to acquire 8 samples on one channel and then interrupt. The interrupt changes the channel selection and starts the next conversion. I am setting port pins high at the start and low at the end of both ISRs to confirm the rate with my scope. ATD0 is generating an interrupt approx. every 112mS (which is the rate I calculated based on the register settings) and ATD1 is about twice that at around 220mS. The ISRs only take about 2-3uS to execute. Does anyone have a clue why ATD1 would behave differently?
 
Here is my initialization function:
 
void Init_ad(void)
{
  /* wrap at AN7 */
  ATD0CTL0 = 0b00000111;
 
  ATD0CTL1 = 0b00000111;
 
  /* turn on A/D & enable interrupt w/ fast flag clearing */
  ATD0CTL2 = ATD0CTL2_ADPU_MASK | ATD0CTL2_AFFC_MASK | ATD0CTL2_ASCIE_MASK;
  /* set for 8 conversions and cause ad to stop when debugging */
  ATD0CTL3 = 0b00000011;
 
  /* set for 10 bit res, 16 AD clock conversion & divide the bus clock by 20 */
  /*
  * This results in approx. 112 uS between interrupts 
  */
  ATD0CTL4 = 0b01101001;
  
  
  /* Start the first conversion */
  ATD0CTL5_DJM = 1; 
 
  /***************** INIT ADC 1 **************************/
  /* wrap at AN7 */
  ATD1CTL0 = 0b00000111;
 
  ATD1CTL1 = 0b00000111;
 
  /* turn on A/D & disable interrupt w/ fast flag clearing */
  ATD1CTL2 = ATD1CTL2_ADPU_MASK | ATD1CTL2_AFFC_MASK | ATD1CTL2_ASCIE_MASK;

  /* set for 8 conversions and cause ad to stop when debugging */
  ATD1CTL3 = 0b00000011;

  /* set for 10 bit res, 16 AD clock conversion & divide the bus clock by 20 */
  /*
  * This results in approx. 225 uS between interrupts
  */
  ATD1CTL4 = 0b01101001;
  
  /* Start the first conversion */
  ATD1CTL5_DJM = 1;  
 
} /* end Init_ad */
Labels (1)
0 Kudos
Reply
3 Replies

1,327 Views
dwhite
Contributor I
Sorry...If you haven't already figured it out, I typed 112mS and 220mS when I meant microseconds not milliseconds.
 
-Dan
0 Kudos
Reply

1,327 Views
kef
Specialist I
ATD1 has 16channels, while ATD0 - 8. All SxC bits set to 0 in ATD0CTL3 mean conversion length is 8, while the same all SxC to 0 in ATD1CTL3 mean conversion length is 16.
0 Kudos
Reply

1,327 Views
dwhite
Contributor I
Thanks. That has fixed it. You blew my mind as I thought that ATD0 and ATD1 were identical. These things should be more clearly documented.
0 Kudos
Reply