9S12DP512 PLL operation

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

9S12DP512 PLL operation

1,589 次查看
astro_goto
Contributor III

Crystal freq is 16 MHz with clock freq 8MHz. I want to boost clock freq to 24 MHz with PLL. Are there any APP notes showing how to do this?  My application is a computer driven telescope  written in assembly language and faster clock speed is needed for all the calculations involved.

Thanx,

astro_goto

标签 (1)
0 项奖励
回复
2 回复数

889 次查看
astro_goto
Contributor III

I found my own solution: PLL operation is not as difficult as I had imagined.

 

The basic calculation isgiven in the Clocks and Generator (CRG) User Guide:

 

PLLCLK = 2 x OSCCLK x [SYNR + 1] / [REFDV + 1]

 

where:

 

    OSCCLK is the crystal frequency: 16MHz in my case which generates a 8MHz bus clock (too slow)

    PLLCLK will be 48MHz to generate a 24MHz bus clock instead of 8MHz

 

Only 5 lines of assembly code are needed to implement the PLL:

 

    movb    #2,SYNR                 ;PLLCLK = 2 * OSCCLK * (SYNR+1)/(REFDV+1)

    movb    #1,REFDV               ;PLLCLK = 2 * 16MHz * (2 + 1)/(1 + 1) = 48MHz
    bset    PLLCTL,#$60           ;PLLON=1, AUTO=1
    brclr    CRGFLG,LOCK,*     ;wait here until PLL is stable and LOCK is set
    bset    CLKSEL,#$80          ;now select PLLCLK/2 as  bus clock (e-clock)

 

For the MC9S12DP512 chip the following definitions apply:

 

   SYNR:        equ     $0034      ;  $ implies hexadecimal number

   REFDV:     equ     $0035

   CLKSEL:   equ     $0039

   PLLCTL:    equ    $003A

   CRGFLG:  equ    $0037

   LOCK:       equ    $08

 

I hope this is helpful to someone.

astro_goto

 

 

 

 

 

 

0 项奖励
回复

889 次查看
MJW
NXP Employee
NXP Employee

Don't forget the filter components on the XFC pin, if you use the PLL on a 0.25 um S12 device.

 

There is a utility available to help with component selection for the filter (to find it type "HCS12PLL" in the "Enter Keyword" search field)

 

Hope that helps.

 

MJW

0 项奖励
回复