尾缀信息

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

尾缀信息

1,544 Views
Chris1616
Contributor II

Hi,

May I ask if these two models are the same product?

If not, can it be completely universal?

 

Model on label: S9S12B128J3CPVE

Model on chip: MC9S12B128CPVE

3 Replies

1,498 Views
lama
NXP TechSupport
NXP TechSupport

Hi,

 these two devices are EXACTLY the same with the same 3L80R mask set .

The device S9S12B128J3CPVE uses automotive format of the part number where the mask set is coded in the part number ...  "J3". If you order this device you will always receive the device with this mask set. It is suitable because the mask set relates to the errata list. (Can be found at device pages)

If you order the device MC..... (general format of part number) then you can get t he device with any possible mask set on stock so your application should be done to implement errata for different mask sets ... if necessary.  In the case of MC9S12B128CPVE you can met also with mask set 0M65G. (This device is the same as S9S12B128F0CFUE ... code F0 for mask set in the art number)

 

Best regards,

Ladislav

0 Kudos
Reply

1,536 Views
Chris1616
Contributor II

{$$YD~RN%0W1`_($3WF27{V.png9W_{VAC$8~GQ~FD~}Z(CNLM.jpg

0 Kudos
Reply

1,542 Views
Chris1616
Contributor II

Please help answer this question. Thank you very much.

0 Kudos
Reply