关于S9S12G128AMLL芯片的静电复位问题

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

关于S9S12G128AMLL芯片的静电复位问题

271 次查看
Bai1
Contributor I

您好:

    在使用贵公司的S9S12G128AMLL芯片时,我们遇到一个关于芯片复位的问题。芯片的复位电路如下图。

复位电路.jpg

          我们的PCB电路板安装在塑料壳内,壳体的盖子使用金属板(金属板固定后等效为浮空金属板),金属板与PCB之间有1cm的距离。在进行静电实验时,我们在金属板上施加6KV的静电,施加静电后会引起芯片复位,我们在芯片的复位引脚处检测到了电压波动,如下图

S9S12G128AMLL复位引脚波形.jpg

 

相同的实验条件下使用相同的复位电路,将S9S12G128AMLL芯片改为其他芯片后也会在复位引脚产生电压扰动,但是不会引起芯片的复位,更换芯片后的复位引脚电压变化如下图。两种芯片的复位引脚收到的扰动是一样的。

更换芯片后引脚波形.jpg

 

我们很疑惑为什么芯片会复位,请问关于S9S12G128AMLL芯片的复位问题应该怎么解决呢?

0 项奖励
回复
1 回复

237 次查看
PavelL
NXP Employee
NXP Employee

Hello,

I can see that voltage on reset pin goes from 3.3V to over 15V. Did you check supply voltage during  your test? Or is there only induced voltage on reset pin?

Best regards,

Pavel

0 项奖励
回复