Will the RapidIot work with an OpenThread border router?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Will the RapidIot work with an OpenThread border router?

Jump to solution
1,790 Views
mrharmonsr
Contributor III

Has anyone tested with an OnepThread border router?

Labels (1)
0 Kudos
Reply
1 Solution
1,658 Views
mrharmonsr
Contributor III

I rebuild the app via the studio and reloaded on my device and the problem went away.

View solution in original post

0 Kudos
Reply
3 Replies
1,658 Views
mrharmonsr
Contributor III

I've set up an openThread boarder router.

On my RapidIoT module I am running the out of box demo.

When I enable thread, the firmware tells me that a reboot is required.

So I reboot.  When the firmware has finished rebooting it tells me a reboot is required.

Again and again and again.

Is this normal for the App?

0 Kudos
Reply
1,659 Views
mrharmonsr
Contributor III

I rebuild the app via the studio and reloaded on my device and the problem went away.

0 Kudos
Reply
1,658 Views
Alexis_A
NXP TechSupport
NXP TechSupport

Dear Larry,

Our stack is compliant with the thread certification. So if the device also is compliant you shouldn't have problems with this. 

Best Regards,

Alexis Andalon

0 Kudos
Reply