Sensors measurement precision

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Sensors measurement precision

1,937 Views
cerny
Contributor II

Hello Eric,

comparison to reference device located at the same place as Rapid IoT kit, five minutes after start of both devices, OOB demo app in Rapid IoT

                           KIT               Reference

temperature :      27                 25.22 C

humidity:             22                 39  %rh

presure:               977              985 hPa

Main diference is humidity, about 50%, how to adjust it ?

Best Regards

Stanislav

Labels (1)
3 Replies

1,782 Views
frq05186
NXP Employee
NXP Employee

Maybe your reference is wrong ?:smileyhappy:

Am joking - we know the sensor measurements into the kit are not accurate. 

That's because the temperature and humidity measured are the ones into the package and are not reflecting 'ambient'

This is also true for air quality and light measurement by the way.

Air is not ciruclating properly into the kit (we wanted to keep it small to develop application)

Light is coming through a hole and is impacted by LEDs into the kit.

For the temperature, we removed an offset (7°) as the self heating (assuming the micro always run at max clock) is repeatable - you would notice a stabilization time assuming you plug a kit whose battery was depleted.

For humidity we did not take any compensation measure as we did not had a proper way to calibrate the humidity measurements vs reality.

1,782 Views
cerny
Contributor II

Thank you Eric, highly appreciated. Some ideas might be helpful for the better temperature adjustment, for instance use temperature measurement on other sensors built in kit or micro bus external devices, for example dust sensor from Maxim have 0.65 C precision temperature sensor as well and located out of MCU heating range, so I believe for our app we could manage temperature measurements also with such a benefit. Multiple sensors availability is also good for various adjustments and reference, would be nice to have such and demo app in Atmo for others. With our app we had limited time to dive in RapidIoT and I highly appreciate your support here, helped a lot! Thanks again!

Stanislav

0 Kudos
Reply

1,782 Views
estephania_mart
NXP TechSupport
NXP TechSupport

Hello, 

Are you having the same behavior on both kits? Is it always before that time? How are you getting the reference? 

Regards,

Estephania 

0 Kudos
Reply