This following example shows the capabilities of the NXP’s RapidIoT to drive the MikroElektronika 8x8 B click module
through the SPI protocol.
This minimalist example to be flashed via MCUXpresso and a docking station embeds only mandatory environment for this application.
The main() is located in the source/ RapidIoT_8x8_B_click_demo_bm.c file
display_decounter(), bright_Configuration(), display_N(), display_X(), display_P(),
scroll_Lines(), scroll_Lines_back(), display_NXP(), display_RapidIoT()
All those functions are used to play with the led matrix.
The code is fully documented.
There is also a readme.txt file located in doc directory that gives you all the information needed to make it works!
Feel free to adapt it to your needs !
Warning: Flashing K64 memory may erase kboot which is ok if you know that you no longer need it -see user guide for more information
Enjoy your RapidIoT!
Thanks for the demo. It helped me in my project. However when I tried to modify it, I faced few issues. It would be helpful if you can take a look into this thread.
Unable to flash new code in rapid iot board
Thanks and Regards
Niranjan
Thank you for sharing Jean-Francois!