Rapid IoT Studio project example: Smart Botanic Garden

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Rapid IoT Studio project example: Smart Botanic Garden

2,561 Views
kenney_q
NXP Employee
NXP Employee

Here is a demo that developed based on the Rapid IoT.

I think you can develop your own project in a short time after read the design user guide

Attachments are :

  • Design user guide: 
    • UG_Rapid IoT Studio project example  Smart Botanic Garden.pdf
  • Video about the project(due to the size limitation, image quality is not so well, please send me your mail address if you want a high quality one) Please open it with 'Windows Media Player'
    • Video_Rapid IoT Studio project example  Smart Botanic Garden.wmv
  • Source code and binary
    • Automatic botanic garden_ firmware.bin
    • Automatic botanic garden.atmo
    • Automatic botanic garden_ source.zip

Project introduction:

An automatic botanic garden can take care of your special plant (e.g. tropical plant);

The humidity, temperature, illumination intensity can be captured then send to your phone by BLE;

User can monitor if the environment is good for plant; 

When the external pump and humidifier are added, user can water the plant/add the humidity remotely. 

pastedImage_1.png

Any issue or not clear, feel free to leave your questions here!

Labels (2)
2 Replies

1,852 Views
jaycanteenwala
NXP Employee
NXP Employee

I really like the block diagram- it shows the major parts of the project at a glance

0 Kudos

1,852 Views
kenney_q
NXP Employee
NXP Employee

Thank you Jay!

Welcome for your comments or improvement suggestion if you have any. :smileyhappy:

0 Kudos