Dear Sir Eric,
Thank you for your nice feedback.
My project is little bit different.
Let me explain you.
This module wifi module has...
1. On-chip PA, LNA, and RF Switch
2. Connection Manager for Autonomous and Fast Wi-Fi Connections
3. Built-in Hardware Crypto Engines for Advanced Security
4 . 16-bit Sigma-Delta ADC : Differential 2 Channels
12-bit SAR ADC : Single-Ended 4 Channels
5. Supports Various Interfaces
– eMMC/SD Expanded Memory
– SDIO Host/Slave Function
– Quad-lane SPI for External Flash Control
– 2 Universal Asynchronous Receivers and Transmitters(UARTs)
– Serial Peripheral Interface(SPI) Master/Slave Interface
– Inter-Integrated Circuit(I2C) Master/Slave Interface
– I2S for Digital Audio Streaming
– Pulse-Width Modulation(PWM)
– Individually Programmable, Multiplexed GPIO Pins
– JTAG
My intention is to use it for security purpose.
This module could be connected with STM32 main MCU where image signal will be processed.
Both will communicate with UART interrupt. Wifi module will be support for AWS(Amazon Web Service) IoT Cloud platform. If you look at the figure, with the GTAG server cloud program will be downloaded.