NTAG 424 NOT DETECTED

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NTAG 424 NOT DETECTED

24,012 Views
kicedric78
Contributor III

Hello, my ntag 424 is not detectable by any NFC device, except put the NDEF message and the reading right on 0E ARE THERE Other configurations for it to be detected by a smartphone?

CC   @Jonathan_Iglesias 

0 Kudos
Reply
9 Replies

23,940 Views
Jonathan_Iglesias
NXP TechSupport
NXP TechSupport

Hi,

as you can see you have modified the write access of the CC file to the NDEF file, the capability container have data  used for NDEF management, so to detect and access NFC Forum defined data, the device has this CC file. 

 

your CC file:                 001720010000FF0406E104010000FF0506E10500808283000000000000000000

new NTAG 424 cc file :001720010000FF0406E104010000000506E10500808283000000000000000000

 you have modified the CC file so there is no write access, 

 
 
 

2020-10-14_15-28-44.png

 you can see this in the NFC forum specification of T4T and in section 8.2.3.2  try to set this back to 00 and perform the NDEF storage. 

BR

 

Jonathan

23,863 Views
kicedric78
Contributor III

ddv

Hello my tests worked on other terminals, I was also able to achieve the objective of @manuel_mertl  thread (https://community.nxp.com/t5/NFC/Configuring-NTAG-424-DNA-with-Encrypted-Part-and-CMAC-Part/m-p/1049315), I will come back in another thread for the rest (ACCES CONTROL system)
THANKS,
0 Kudos
Reply

23,972 Views
kicedric78
Contributor III

the cc files picture

0 Kudos
Reply

23,992 Views
kicedric78
Contributor III

1.png2.png3.png

0 Kudos
Reply

23,983 Views
Jonathan_Iglesias
NXP TechSupport
NXP TechSupport

@kicedric78 ,

can you confirm that you have done the steps I explain in the following steps ?

https://community.nxp.com/t5/NFC/Change-Keys-and-quot-lock-quot-NTAG-DNA-424/m-p/1058611#M7162

 

https://community.nxp.com/t5/NFC/Configuring-NTAG-424-DNA-with-Encrypted-Part-and-CMAC-Part/m-p/1049...

 

also please share the value of the capability container file, 

jonathaniglesia_0-1602624499076.png

to check if you have changes the read access conditions.

Br

 

Jonathan

 

23,978 Views
kicedric78
Contributor III
yes I understand the method used in this thread https://community.nxp.com/t5/NFC/Configuring-NTAG-424-DNA-with-Encrypted-Part-and-CMAC-Part/m-p/1049315
but I just want to launch the browser of the smartphone (simple url) is this config necessary?
0 Kudos
Reply

23,956 Views
Jonathan_Iglesias
NXP TechSupport
NXP TechSupport

if you dont want a SUN inside your tag, just a simple URL, it is very simple:

if you are using TagXplorer  do the following:

  1.  Connect  reader
  2.  connect tag and then go to NDEF operations
  3.  write NDEF
  4.  +url
  5.  fill the information
  6.  write tag
  7. see successful message

jonathaniglesia_0-1602683858079.png

after this the tag should be able to  be read by a phone, this is done if you have not modified anything to the tag, if you have changed the access conditions of the tag or something you should first authenticate, also be sure that you have not modified the CC file, this fille will tell the phone the memory, the reading rights and write rights, and other information you can see in the DS. 

BR

 

Jonathan

23,949 Views
kicedric78
Contributor III

okay no modification for the reader apart from activating the nfc? I'm going to change my smartphone to see

0 Kudos
Reply

23,987 Views
Jonathan_Iglesias
NXP TechSupport
NXP TechSupport

Hi kicedric78,

Hope you are doing great, can you share the NDEF and Capability container file settings and the capability container file value.

Have a great day !
BR

Jonathan