Large custom NFC tags / antennas

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Large custom NFC tags / antennas

2,631 Views
shanehill00
Contributor I

Currently, I am doing research, assessing feasibility and building a prototype of an NFC based product. I am discovering that the form factor for commonly available NFC tags are not going to meet my needs. So I need to start looking at something custom.

I am not an expert in the NFC field and I am still in early stages of research but I am quite serious about getting this done. Also, I have made prototypes that do work but like I mentioned above, the commonly available tags will not meet my form factor requirements.

The basic parameters of my needs are as follows:

1) Need to be able to operate on carbon fiber and metal (ferrite backed tags work in my testing)

2) I need the tag/antenna to operate over a large field. I am currently working with antennas of 45mm x 100mm

3) Ultimately, the tags will be inlaid into vinyl sheets 10-12 mils thick

Can someone help me understand how I would go about getting tags that fit the above requirements?

Labels (1)
0 Kudos
Reply
0 Replies