How is the Rapid Iot sensor data sent to the cloud?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How is the Rapid Iot sensor data sent to the cloud?

ソリューションへジャンプ
1,959件の閲覧回数
mrharmonsr
Contributor III

I would like to understand the connectivity of the Rapid Iot kit.  Where can I find documentation?

I can provision and connect to the Rapid Iot from my iPhone.  I assume this is a BLE connection.

(Awfully  inconvenient having to re-provision every time I use the device)

When I connect to the website via a browser I can see data using a quick glance widgit.

(However I can't get date from the Rapid IOT application and the graph feature works intermittently)

Is my iPhone routing the sensor data to the cloud?

ラベル(1)
0 件の賞賛
返信
1 解決策
1,828件の閲覧回数
theophileleroy
NXP Employee
NXP Employee

Yes, the phone is receiving data from the kit via BLE and send them to the cloud over Wifi connection or hotspot.

This scenario is one of the behaviors described in the factory sheet available on the product page documentation.

pastedImage_1.png

Moreover, you will find documentation of the connectivity part of Rapid-IoT in the Software Development Kit available in the Software&Tool under the path: SLN-RPK-NODE-SDK\SDK_2.2_RapidIoT_MKW41Z4\docs\wireless".

Regards,

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,829件の閲覧回数
theophileleroy
NXP Employee
NXP Employee

Yes, the phone is receiving data from the kit via BLE and send them to the cloud over Wifi connection or hotspot.

This scenario is one of the behaviors described in the factory sheet available on the product page documentation.

pastedImage_1.png

Moreover, you will find documentation of the connectivity part of Rapid-IoT in the Software Development Kit available in the Software&Tool under the path: SLN-RPK-NODE-SDK\SDK_2.2_RapidIoT_MKW41Z4\docs\wireless".

Regards,

0 件の賞賛
返信