I'm using FRWY-LS1012A as a starting board and I am adding more parts for my custom design. I am trying to source the parts to build this board. But some of parts I can not find the vendor/manufacturer to buy the parts in. Can NXP please help (please also see attached the parts I'm having trouble with). Please let me know where I can buy these parts?
Thank you,
Hung
---
Value | Reference | Description | Manufacturer | P/N |
USB3_MICRO_AB | J5 | CON 10 USB MICRO-AB 3.0 SKT RA SMT 0.65MM SP 106H AU | ANYTRONIC CORPORATION LIMITED | 23H90601#LCP-582LF |
HDR 2X5 | J9,J10 | HDR 2X5 TH 50MIL CTR 167H AU 91L | ANYTRONIC CORPORATION LIMITED | 0922S0205011N6T-2LF |
23HG0101#LCP-702LF | J11 | CON 5 USB2.0 MICRO-AB RA REVERSE SKT SMT 0.65MM SP 128H AU | ANYTRONIC CORPORATION LIMITED | 23HG0101#LCP-702LF |
CON_1X8 | J33,J34 | CON 1X8 SKT TH 100MIL SP 344H AU 394L | ANYTRONIC CORPORATION LIMITED | 08001S3 0811-100-29LF |
M.2 SKT | J35 | CON 67 PCI EXPRESS M.2 CRD KEY- E SKT RA SMT 0.5MM SP 165H AU | ANYTRONIC CORPORATION LIMITED | 1J0E 42010R-2LF |
95220030-14RRF | J36 | CON 8 SKT SD/MMC RA SMT 43MIL SP 84H AU | ANYTRONIC CORPORATION LIMITED | 95220030-14RLF |
HDR 1X2 TH | J37 | HDR 1X2 TH 100MIL SP 339H AU 98L | ANYTRONIC CORPORATION LIMITED | 090021S02015-2LF |
3520N811001-14LF | J39 | CON RJ45 SHLD RA TH 81 SP 593H AU 104L | ANYTRONIC CORPORATION LIMITED | 3520N811001-14LF |
4.7uH | L11,L12 | IND PWR 4.7uH@1MHZ 1.1A 20% 2020 | Shenzhen Sunlord Electronics Co., Ltd | SPH202012H4R7MT |
120OHM | L14,L15,L18,L24,L88 | IND FER BEAD 120OHM@100MHZ 2A 25% 0603 | Shenzhen Sunlord Electronics Co., Ltd | PZ1608U121-2R0TF |
W25M161AWEIT | U11 | IC MEM FLASH 16M-BIT SERIAL NOR + 1G-BIT SERIAL NAND 1.7-1.95V WSON-8 | WINBOND ELECTRONICS CORP | W25M161AWEIT |
LS1012A | U14 | IC MPU LS1012A 1000MHZ LGA211 | FREESCALE SEMICONDUCTOR | LS1012AXE7KKB |
AR8033 | U16,U17 | IC XCVR ETHERNET PHY 10/100/1000 Mbps 3.3V QFN48 | Qualcomm Atheros, Inc | AR8033-AL1A |
Find information about parts from ANYTRONIC CORPORATION LIMITED on the following web:
http://www.anytronic.com.tw/Products.asp
Use the first indexes in parts for selection on this web.
Find information about parts from Shenzhen Sunlord Electronics Co., Ltd on the following web:
http://www.sunlordinc.com/searchpn.aspx
See information about the W25M161AWEIT part on Winbond web:
https://www.winbond.com/resource-files/w25m161av%20combo%20reva%20091317%20mod%20final.pdf
Use the following NXP page about the LS1012a:
Use the following document for the AR8033:
http://microchip.ho.ua/data/AR8033.pdf
Have a great day,
Pavel Chubakov
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------