Empty frame received on ethernet of MIMXRT1062

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Empty frame received on ethernet of MIMXRT1062

5,067件の閲覧回数
Sha_G
Contributor I

The " ENET_GetRxFrameSize "show that the length of the received frame is 0. The ' control ' element of the ' curBuffDescrip ' always comes as 32768 and as a result ' kStatus_ENET_RxFrameEmpty ' is returned.

The transmit routines work fine and frames are transmitted correctly.

But do not see any frames received because of the above observations.

0 件の賞賛
返信
3 返答(返信)

5,034件の閲覧回数
Sha_G
Contributor I

I am replicating the " enet_txrx_transfer " example from the SDK on our board. Just changed the pin numbers for INT and RST as per our board. This example works fine on the EVK board. 

However, I see that on our board the " PHY_KSZ8081_GetAutoNegotiationStatus() " and the " PHY_KSZ8081_GetLinkStatus() " do not read the Basic Status register of the KSZ8081 correctly. As a result The program cannot detect link status / receive frames / auto negotiate. 

0 件の賞賛
返信

5,025件の閲覧回数
FelipeGarcia
NXP Employee
NXP Employee

Hi,

If the same code with no major modification is not working in custom board then I think this could be a hardware related issue. You can see our schematics of the evaluation board as reference from this link: https://www.nxp.com/webapp/Download?colCode=MIMXRT1060-EVK-DESIGNFILE-A3

Best regards,

Felipe

0 件の賞賛
返信

5,049件の閲覧回数
FelipeGarcia
NXP Employee
NXP Employee

Hi,

Are you using SDK example? If so, could you please specify? Also provide steps to replicate this in our EVK.

Best regards,

Felipe

0 件の賞賛
返信