Device does not enumerate as a mass storage device.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Device does not enumerate as a mass storage device.

1,207件の閲覧回数
n5kzw
Contributor I

I can get the Rapid IoT Prototyping Kit into download mode using either of the two methods shown, but it is not enumerated as a mass storage device either on my Windows 10 laptop, or on the Ubuntu 18.04 desktop.  Neither computer gives any sort of indication that a USB device has been added or removed regardless of whether the Rapid IoT is in dowload mode or normal mode.  It does not show up in Windows Device Manager, or Linux lsusb.

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,057件の閲覧回数
theophileleroy
NXP Employee
NXP Employee

Please find a video exaplaning the sequence of action to enter mass storage mode:

https://community.nxp.com/docs/DOC-342335 

Make sure to keep hloding for 2 sec SW3 button after releasing reset.

If this still doesn't work you can try to recover default binaries of rapid-iot:

Recovering k64f & kw41z applications binaries 

https://community.nxp.com/docs/DOC-342112 

Regards,

0 件の賞賛
返信