Device does not enumerate as a mass storage device.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Device does not enumerate as a mass storage device.

1,153 Views
n5kzw
Contributor I

I can get the Rapid IoT Prototyping Kit into download mode using either of the two methods shown, but it is not enumerated as a mass storage device either on my Windows 10 laptop, or on the Ubuntu 18.04 desktop.  Neither computer gives any sort of indication that a USB device has been added or removed regardless of whether the Rapid IoT is in dowload mode or normal mode.  It does not show up in Windows Device Manager, or Linux lsusb.

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

1,003 Views
theophileleroy
NXP Employee
NXP Employee

Please find a video exaplaning the sequence of action to enter mass storage mode:

https://community.nxp.com/docs/DOC-342335 

Make sure to keep hloding for 2 sec SW3 button after releasing reset.

If this still doesn't work you can try to recover default binaries of rapid-iot:

Recovering k64f & kw41z applications binaries 

https://community.nxp.com/docs/DOC-342112 

Regards,

0 Kudos
Reply