DPS in Azure SDK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DPS in Azure SDK

2,085 Views
pritesh_shah
Contributor I

Hello,

I need to provision the kinetis k64 based device with the Azure portal. so
I have downloaded an SDK for Kinetis K64.

I have seen the example to connect the device with the Azure cloud.
But I did not find support for auto-provisioning of the device with Azure cloud.
SDK does not include support for Device Provisioning Service.

Please guide me on how I can achieve the zero-touch provisioning with Azure cloud
and provide the sample example for that.

Tags (2)
0 Kudos
Reply
1 Reply

1,969 Views
Sabina_Bruce
NXP Employee
NXP Employee

Hello Pritesh,

Hope you are doing well.

Any implementation of different features must be done by our customers. We do not have examples using the K64 for zero touch provisioning. I recommend that you check the following documentation that will help you as a reference on how to get started. 

Overview of Azure IoT Hub Device Provisioning Service | Microsoft Docs 

Set up IoT Hub Device Provisioning Service in the Azure portal | Microsoft Docs 

https://community.nxp.com/docs/DOC-329718 

Hope it helps!

Sabina

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

----------------------------------------------------------------------------------------------------------------------- 

0 Kudos
Reply