Azure IoT Middleware support in k8x series

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Azure IoT Middleware support in k8x series

1,482 次查看
pritesh_shah
Contributor I

Hi,

We are developing an application using kinetis controller which required features of an azure IoT.

while selecting an azure IoT middleware component in "MCUxpresso software development kit", it is not showing the k8x series controllers in the whitelist.

So Need to confirm that Azure IoT is supported or not in k8x series.

标记 (2)
0 项奖励
回复
1 回复

1,373 次查看
Sabina_Bruce
NXP Employee
NXP Employee

Hello,

According to Azure IoT documentation on their website it can be used with the microcontroller. You were not able to find it in the SDK builder, because there has not been an implementation or development of examples utlizing this specific microcontroller from our teams. The implementation and usage in custom applications will have to be developed by the customer.

Best Regards,

Sabina