why the P2010 cannot be JTAG up, the information as follows testing for target STOP State...............Failed when make the scan_mode signal pull to 3.3V directly, the JTAG can be up occasionally the power on reset sequency is successful, because the

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

why the P2010 cannot be JTAG up, the information as follows testing for target STOP State...............Failed when make the scan_mode signal pull to 3.3V directly, the JTAG can be up occasionally the power on reset sequency is successful, because the

723 Views
hit_zhangqi
Contributor I

why the P2010 cannot be JTAG up, the information as follows
testing for target STOP State...............Failed

when make the scan_mode signal pull to 3.3V directly, the JTAG can be up occasionally

the power on reset sequency is successful, because the ready signal is assert and the asleep signal is deassert

Tags (1)
0 Kudos
2 Replies

593 Views
shengxian_ma
Contributor I

have you solved this question, I met it  too...    p2020 testing for target STOP State...............Failed

0 Kudos

593 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please refer to the following JTAG interface hardware design.

pastedImage_1.png

In addition, please create a bareboard project in CodeWarrior and enable JTAG diagnostics function in CodeWarrior IDE, please refer to the following procedure to capture CCS log in the IDE.

 

please enable CCS log from "Run->Debug Configurations-><project>-core0_RAM_<processor>-Connect(Download)->Edit...->Advanced->Advanced CCS setting->Enable logging", and connect to the target from "Run->Debug Configurations-><project>-core0_RAM_<processor>-Connect(Download)->Debug”, the CCS log will be displayed in the console panel in CodeWarrior IDE.
If the CCS log in the console is truncated, please enlarge the console buffer from Window->Preferences->Run/Debug->Console->uncheck "Limit console output".
(Please open the console panel from Window->Show View->Console, and if nothing displayed, please choose the correct session on the right top icon in the panel.)


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos