what is the JTAG instruction register length for the T2080

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

what is the JTAG instruction register length for the T2080

Jump to solution
1,392 Views
kbell_hardware
Contributor III

I know the IDCODE is 32 bits but that doesn't mean the IR length is the same. This does not appear to be in the documentation and the tcl scripts just use "t2080" because that info is built in somewhere.

0 Kudos
Reply
1 Solution
1,071 Views
ufedor
NXP Employee
NXP Employee

The T2080 JTAG IR length is 8 bit.

View solution in original post

1 Reply
1,072 Views
ufedor
NXP Employee
NXP Employee

The T2080 JTAG IR length is 8 bit.