unable to program spi flash in p1022

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

unable to program spi flash in p1022

839 Views
somyaaggarwal08
Contributor II

Hi,

I am trying to program spi based flash device ie micron N25q256a using jtag interface in p1022 based board. However i get an error flash algorithm did not execute completely.I have also attached script file.Could you suggest any possible reason of this?

The error appears after execution of line "FLASHFILE.TARGET 0x10001000++0x1FFF  0x10003000++0x1FFF  ~~/demo/powerpc/flash/byte/spi64fs_ppcpq.bin"

Original Attachment has been moved to: flash_spi.cmm.zip

0 Kudos
Reply
1 Reply

737 Views
alexander_yakov
NXP Employee
NXP Employee

Which software you are using to program SPI flash?

0 Kudos
Reply