u-boot-ls1-2015.01 build issue with gcc-5 in sdk-v1.8

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

u-boot-ls1-2015.01 build issue with gcc-5 in sdk-v1.8

2,028件の閲覧回数
skrishnakar
Contributor III

Hello Yiping,

I am trying to build u-boot-ls1_2015.01 from SDK-v1.8 for LS1, but facing strange build issue during linking stage. The same u-boot builds fine with gcc-4.9.2 in my old setup. The following is the error seen at the end of compilation :

|   arm-none-linux-gnueabi-gcc  --sysroot=/home/srikanth/cedar/ls1/build/tmp/sysroots/ls1021atwr -Wp,-MD,examples/standalone/.hello_world.o.d  -nostdinc -isystem /home/srikanth/mgc/embedded/codebench/bin/../lib/gcc/arm-none-linux-gnueabi/5.2.0/include -Iinclude  -I../include -I../arch/arm/include -include ../include/linux/kconfig.h  -I../examples/standalone -Iexamples/standalone -D__KERNEL__ -D__UBOOT__ -DCONFIG_SYS_TEXT_BASE=0x67f80000 -Wall -Wstrict-prototypes -Wno-format-security -fno-builtin -ffreestanding -Os -fno-stack-protector -g -fstack-usage -Wno-format-nonliteral -Werror=date-time -fno-toplevel-reorder -D__ARM__ -marm -mno-thumb-interwork -mabi=aapcs-linux -mword-relocations -march=armv7-a -mno-unaligned-access -ffunction-sections -fdata-sections -fno-common -ffixed-r9 -msoft-float -pipe    -D"KBUILD_STR(s)=#s" -D"KBUILD_BASENAME=KBUILD_STR(hello_world)"  -D"KBUILD_MODNAME=KBUILD_STR(hello_world)" -c -o examples/standalone/hello_world.o ../examples/standalone/hello_world.c

|   arm-none-linux-gnueabi-ld.bfd     -r -o examples/standalone/libstubs.o examples/standalone/stubs.o

|   arm-none-linux-gnueabi-ld.bfd   -g -Ttext 0xc100000 -o examples/standalone/hello_world -e hello_world examples/standalone/hello_world.o examples/standalone/libstubs.o -L /home/srikanth/mgc/embedded/codebench/bin/../lib/gcc/arm-none-linux-gnueabi/5.2.0 -lgcc

|   arm-none-linux-gnueabi-objcopy -O srec  examples/standalone/hello_world examples/standalone/hello_world.srec

|   arm-none-linux-gnueabi-objcopy -O binary  examples/standalone/hello_world examples/standalone/hello_world.bin

|   arm-none-linux-gnueabi-ld.bfd   -pie  --gc-sections -Bstatic -Ttext 0x67f80000 -o u-boot -T u-boot.lds arch/arm/cpu/armv7/start.o --start-group  arch/arm/cpu/built-in.o  arch/arm/cpu/armv7/built-in.o  arch/arm/lib/built-in.o  board/freescale/common/built-in.o  board/freescale/ls1021atwr/built-in.o  common/built-in.o  disk/built-in.o  drivers/built-in.o  drivers/dma/built-in.o  drivers/gpio/built-in.o  drivers/i2c/built-in.o  drivers/mmc/built-in.o  drivers/mtd/built-in.o  drivers/mtd/onenand/built-in.o  drivers/mtd/spi/built-in.o  drivers/net/built-in.o  drivers/net/phy/built-in.o  drivers/pci/built-in.o  drivers/power/built-in.o  drivers/power/battery/built-in.o  drivers/power/fuel_gauge/built-in.o  drivers/power/mfd/built-in.o  drivers/power/pmic/built-in.o  drivers/serial/built-in.o  drivers/spi/built-in.o  drivers/usb/eth/built-in.o  drivers/usb/gadget/built-in.o  drivers/usb/host/built-in.o  drivers/usb/musb-new/built-in.o  drivers/usb/musb/built-in.o  drivers/usb/phy/built-in.o  drivers/usb/ulpi/built-in.o  fs/built-in.o  lib/built-in.o  net/built-in.o  test/built-in.o  test/dm/built-in.o --end-group arch/arm/lib/eabi_compat.o  -L /home/srikanth/mgc/embedded/codebench/bin/../lib/gcc/arm-none-linux-gnueabi/5.2.0 -lgcc -Map u-boot.map

|   arm-none-linux-gnueabi-objcopy  -j .text -j .secure_text -j .rodata -j .hash -j .data -j .got.plt -j .u_boot_list -j .rel.dyn --gap-fill=0xff -O srec u-boot u-boot.srec

|   arm-none-linux-gnueabi-objcopy  -j .text -j .secure_text -j .rodata -j .hash -j .data -j .got.plt -j .u_boot_list -j .rel.dyn --gap-fill=0xff -O binary  u-boot u-boot.bin

| /home/srikanth/mgc/embedded/codebench//bin/arm-none-linux-gnueabi-objcopy:u-boot.bin[.text]: No space left on device

| make[1]: *** [u-boot.bin] Error 1

Could you kindly help us fix this issue ? I did see an upstream patch of changing "TEXT_BASE" from upstream for LS1:

git.denx.de Git - u-boot.git/blobdiff - include/configs/ls1021atwr.h

This didn't seem to help, even upstream u-boot (denx) 2015.10-rc3 also failed to build with same error for LS1 using GCC-5.2 toolchain.

Your inputs are appreciated.

Thanks!

Srikanth

0 件の賞賛
返信
3 返答(返信)

1,557件の閲覧回数
abdurrehman
Contributor III

I am experiencing a similar error while trying to build u-boot-qoriq_2015.01 from QorIQ SDK v1.8 with gcc version 5.2.0. Same u-boot builds fine with gcc 4.9.1.

Following error is breaking the compilation:

|   LD      examples/standalone/hello_world

|   OBJCOPY examples/standalone/hello_world.srec

|   OBJCOPY examples/standalone/hello_world.bin

|   LD      examples/standalone/sched

|   OBJCOPY examples/standalone/sched.srec

|   OBJCOPY examples/standalone/sched.bin

|   LD      u-boot

|   OBJCOPY u-boot.srec

|   OBJCOPY u-boot.bin

| /var/arehman/mgc/embedded_ppc/codebench//bin/powerpc-linux-gnu-objcopy:u-boot.bin[.u_boot_list]: No space left on device

| make[1]: *** [u-boot.bin] Error 1

0 件の賞賛
返信

1,557件の閲覧回数
Pavel
NXP Employee
NXP Employee

Use the following command sequence for u-boot modification:

1) bitbake -c cleanall u-boot

2) bitbake -c patch u-boot // source of the u-boot

U-boot source is available using the following path:

QorIQ-SDK-V1.7-20141218-yocto_RDS_20150302/build_p2020rdb_release/tmp/work/p2020rdb-fsl-linux-gnuspe/u-boot-qoriq/2014.07+fslgit-r0/git

3) bitbake u-boot                // build new u-boot binary image

Usually the following command sequence provides correct using of the SDK under Ubuntu 12 Ubuntu 14:

  1. 1. sudo apt-get install ubuntu-minimal ubuntu-standard patch vim-common sed wget subversion git-core coreutils libbonobo2-common unzip texi2html texinfo libsdl1.2-dev docbook-utils gawk python-pysqlite2 diffstat make gcc build-essential xz-utils g++ desktop-file-utils chrpath libgl1-mesa-dev libglu1-mesa-dev autoconf automake groff libtool xterm libncurses5-dev cvs tofrodos

if it is 64-bit operating system, run the following command also:

sudo apt-get install ia32-libs lib32ncurses5

  1. 2. sudo dpkg-reconfigure dash

then choose "No" and you're done. )

  1. 3. install SDK for your core (500V2)
  2. 4. install SDK source
  3. 5. sudo ./poky/scripts/host-prepare.sh

  1. 6. usually Linux recommends also run the following command: sudo usr/sbin/visudo

  1. 7. $ source ./poky/fsl-setup-poky <-m machine> [-j threads] [-t tasks] [-l]

$ bitbake <task-name>


Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,557件の閲覧回数
skrishnakar
Contributor III

Pavel,

NOTE:  Affected platforms: ARM (LS1) & PowerPC (Qoriq u-boot-2015.01)

Thanks for your response. I am talking about freescale Layerscape TWR-LS1021A Arm platform. I am building the u-boot from u-boot-qoriq git repo - sdk-v1.8 branch, using ls1021atwr_nor_defconfig.

Could you try building u-boot-ls1_2015.01.bb with GCC 5.x and let me know, if it builds ?

Thanks!

0 件の賞賛
返信