Does the software exist for u-boot somewhere? Specifically this question is for Layerscape and QorIQ.
Yes, I saw this patch. The board is recognizing the AQR107 part but the AQR107 does not operate unless it gets a firmware download.
=> mdio list
FSL_MDIO0:
0 - Marvell 88E1510 <--> FM1@DTSEC2
1 - Marvell 88E1510 <--> FM1@DTSEC1
2 - Marvell 88E1111S <--> FM1@DTSEC4
3 - Marvell 88E1111S <--> FM1@DTSEC5
4 - Aquantia AQR107 <--> FM1@DTSEC3
=>
There are two options for firmware download: “MDIO Bootload” or program the attached SPI FLASH device. I was looking to see if the “MDIO Bootload” was supported in u-boot.
Thanks
Greg
Have a great day,
Pavel Chubakov
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------