u-boot AQR107 firmware download - MDIO Bootload

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

u-boot AQR107 firmware download - MDIO Bootload

1,610 Views
Davisg
Contributor III

Does the software exist for u-boot somewhere? Specifically this question is for Layerscape and QorIQ.

0 Kudos
Reply
2 Replies

1,189 Views
Davisg
Contributor III

Yes, I saw this patch. The board is recognizing the AQR107 part but the AQR107 does not operate unless it gets a firmware download.

=> mdio list

FSL_MDIO0:

0 - Marvell 88E1510 <--> FM1@DTSEC2

1 - Marvell 88E1510 <--> FM1@DTSEC1

2 - Marvell 88E1111S <--> FM1@DTSEC4

3 - Marvell 88E1111S <--> FM1@DTSEC5

4 - Aquantia AQR107 <--> FM1@DTSEC3

=>

There are two options for firmware download: “MDIO Bootload” or program the attached SPI FLASH device. I was looking to see if the “MDIO Bootload” was supported in u-boot.

Thanks

Greg

0 Kudos
Reply

1,189 Views
Pavel
NXP Employee
NXP Employee

Look at the following page about patch to support Aquantia AQR107 in LS1043A:

https://community.nxp.com/docs/DOC-332265


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply