I have enabled the 1G ethernet ports on the t2080 reference board, assigned IP address. However, I am unable to ping to the board from a computer attached to the network. I have tried eth2/3/4/5 interfaces, none of them seem to be working.
Attached are the kernel boot up and Uboot logs.
PS: I see there are similar queries, but not solution suggested..
Original Attachment has been moved to: bootuplogs.zip
In your logs I see two different hardware interfaces have the same MAC address:
Here is a part of your boot log, interfaces with the same MAC are marked by bold:
fsl_mac: fsl_mac: FSL FMan MAC API based driver
fsl_mac ffe4e0000.ethernet: FMan MEMAC
fsl_mac ffe4e0000.ethernet: FMan MAC address: 00:04:9f:04:e3:d6
fsl_mac ffe4e2000.ethernet: FMan MEMAC
fsl_mac ffe4e2000.ethernet: FMan MAC address: 00:04:9f:04:e3:d3
fsl_mac ffe4e4000.ethernet: FMan MEMAC
fsl_mac ffe4e4000.ethernet: FMan MAC address: 00:04:9f:04:e3:d4
fsl_mac ffe4e6000.ethernet: FMan MEMAC
fsl_mac ffe4e6000.ethernet: FMan MAC address: 00:04:9f:04:e3:d5
fsl_mac ffe4f0000.ethernet: FMan MEMAC
fsl_mac ffe4f0000.ethernet: FMan MAC address: 00:04:9f:04:e3:d6
fsl_mac ffe4f2000.ethernet: FMan MEMAC
fsl_mac ffe4f2000.ethernet: FMan MAC address: 00:04:9f:04:e3:d7
This is obviously incorrect situation, please fix and check again.
Please show "ifconfig -a" for further debugging.
Have a great day,
Alexander
TIC
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thanks. !