"CPU up timeout. CPU up mask is 7 should be f" issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

"CPU up timeout. CPU up mask is 7 should be f" issue

2,458 Views
gyosunshim
Contributor III

Hi All,

It has a T2081 board.

There is a T2081 with eight cores, it does recognize eight of the boot boot logo, as shown below.

Assemble the two were the same board like that this phenomenon appears in one board.

Because of this problem should have access to the shell.

A hardware fault would not be any part of this phenomenon appear?

fail boot log, board-a

...

CPU up timeout. CPU up mask is 7 should be f

...

e6500 family performance monitor hardware support registered

Processor 6 is stuck.

smp_85xx_kick_cpu: Can not start CPU #7. Start CPU #6 first.

smp: failed starting cpu 7 (rc -2)

Brought up 6 CPUs

pass boot log, board-b

e6500 family performance monitor hardware support registered

Brought up 8 CPUs

Thanks,

Best regards,

Gyosun.

0 Kudos
Reply
9 Replies

2,090 Views
ufedor
NXP Employee
NXP Employee

Please provide PVR and SVR values for the processors on both boards.

Ensure that IFC_A[16:20] are not pulled down during power-on reset. This pin may be pulled up, driven high, or if there are any connected devices, left in tristate. If this pin is connected to a device that pulls down during reset, an external pull-up is required to drive this pin to a safe state during reset.

0 Kudos
Reply

2,090 Views
gyosunshim
Contributor III

Hello ufedor,

Both boards have the same value.

=> md.l ffe0e0000 32

fe0e0000: 207bff7f ff000000 00000000 00000000     {..............

fe0e0010: 00000000 00000000 00000000 00000000    ................

fe0e0020: ff000000 00000000 24000000 00000000    ........$.......

fe0e0030: 00000000 00000000 00000000 00000000    ................

fe0e0040: 00000000 00000000 00000000 00000000    ................

fe0e0050: 00000000 00000000 00000000 00000000    ................

fe0e0060: 00000000 00000000 00000000 00000000    ................

fe0e0070: 00000200 00000000 00000000 00000000    ................

fe0e0080: 00000000 00000000 00000000 00000000    ................

fe0e0090: 00000000 00000000 00000000 00000000    ................

fe0e00a0: 80400120 85310011 00000040 00000000    .@. .1.....@....

fe0e00b0: 00000000 00000000 00000000 00000000    ................

fe0e00c0: 00004000 00000000                      ..@.....

=>

All are pulled up.

IFC_A_20_16.png

Thanks,

Gyosun.

0 Kudos
Reply

2,090 Views
ufedor
NXP Employee
NXP Employee

Please provide complete U-Boot and Linux boot logs for both boards.

Use a digital scope to verify IFC_A[16:20] behaviour during POR on the problem board.

0 Kudos
Reply

2,090 Views
gyosunshim
Contributor III

Hello ufedor,

Attach boot log file of both boards.

When the POR and the IFC_A[16:20] signal to the digital scope as follows. Both are identical.

IFC_A_20_16_timing.png

I saw the same symptoms again, replace the CPU.

Thanks,
Best regards,

Gyosun.

0 Kudos
Reply

2,090 Views
ufedor
NXP Employee
NXP Employee

Please provide raw memory dumps of CCSR area containing all DDR controller registers (offset 0x00_8000 - 0x00_8FFF) for proper and failing cases.

0 Kudos
Reply

2,090 Views
gyosunshim
Contributor III

Hello ufedor,

DDR registers all the data dump has been attached.

Another difference is not visible.

Thanks,

Gyosun.

0 Kudos
Reply

2,090 Views
ufedor
NXP Employee
NXP Employee

It will be more convenient to investigate the issue as technical case:

How I could create a Service Request?

0 Kudos
Reply

2,090 Views
gyosunshim
Contributor III

Thank you for your help.

But the problem has not yet been resolved.

With the help of others better.

Thank you.

Best regards,

Gyosun.

0 Kudos
Reply

2,090 Views
ufedor
NXP Employee
NXP Employee

Please note that the investigated issue is not general - it is specific to the sigle board.

This is why it was recommended to create a technical case.

0 Kudos
Reply