qoriq linux fetch failure from git://git.freescale.com/ppc/sdk/linux.git

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

qoriq linux fetch failure from git://git.freescale.com/ppc/sdk/linux.git

927 Views
tombeaman
Contributor I

this is the error I see

git clone git://git.freescale.com/ppc/sdk/linux.git

017/05/09 14:36:13 socat[72207] E CONNECT git.freescale.com:9418: Service Unavailable
fatal: Could not read from remote repository.

any idea why this is happening, it has worked for me in the past

0 Kudos
Reply
1 Reply

817 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Tom Beaman,

I can clone git://git.freescale.com/ppc/sdk/linux.git from the internal, however it has not been updated to the latest.

Please check whether you could access http://sw-stash.freescale.net/projects/SDK/repos/linux-sdk2.0/browse from the external, please click "Actions" on the left to clone the latest source code. We all use this.


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply